AXIS#.SWLS.LIMIT#

Description

Sets the position value for a software limit switch, LIMIT0 or LIMIT1.

Examples

Usage

If only one limit switch is enabled, AXIS#.SWLS.EN = 1 or 2, then AXIS#.SWLS.LIMIT0 is the lower limit and AXIS#.SWLS.LIMIT1 is the upper limit.

If both limit switches are enabled, AXIS#.SWLS.EN = 3, then whichever switch is set to a larger value is the upper limit switch and the other switch is the lower limit switch.

"AXIS#.CS.DEC " is executed when a SWLS is triggered. The user can set the CS.DEC value, or go with the default 10,000 rpm/s. Once the switch is triggered, a warning W6006 results, and the position/load must be moved back within the limits to remove the warning.

Code

Axis 1 lower limit switch set to 1000 and upper limit switch set to 5000. Axis 1 home position is set and then both software limit switches are enabled.

-->AXIS1.SWLS.LIMIT0 1000
-->AXIS1.SWLS.LIMIT1 5000
-->AXIS1.HOME.SET
-->AXIS1.SWLS.EN 3

Context

For more information on limit switches, refer to Limits.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units Position Units
Range -9,007,199,254,740,992.000 to 9,007,199,254,740,992.000
Default Value AXIS#.SWLS.LIMIT0 = 0
AXIS#.SWLS.LIMIT1 = 5760
Data Type Float
See Also AXIS#.SWLS.STATE, AXIS#.SWLS.EN
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SWLS.LIMIT0

500fh

03h

Signed32

Position

-

Read/Write

No

AXIS1.SWLS.LIMIT1

500fh

04h

Signed32

Position

-

Read/Write

No

AXIS2.SWLS.LIMIT0

510fh

03h

Signed32

Position

-

Read/Write

No

AXIS2.SWLS.LIMIT1

510fh

04h

Signed32

Position

-

Read/Write

No

AXIS1.SWLS.LIMIT0

607dh

01h

Signed32

Position

-

Read/Write

No

AXIS1.SWLS.LIMIT1

607dh

02h

Signed32

Position

-

Read/Write

No

AXIS2.SWLS.LIMIT0

687dh

01h

Signed32

Position

-

Read/Write

No

AXIS2.SWLS.LIMIT1

687dh

02h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6501

1

6501 (0x1965)

AXIS1.SWLS.LIMIT0

Signed32

Read/Write

Yes

72037

2

6501 (0x1965)

AXIS2.SWLS.LIMIT0

Signed32

Read/Write

Yes

6502

1

6502 (0x1966)

AXIS1.SWLS.LIMIT1

Signed32

Read/Write

Yes

72038

2

6502 (0x1966)

AXIS2.SWLS.LIMIT1

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SWLS.LIMIT0

6501

Signed32

Read/Write

Position

AXIS#.SWLS.LIMIT1

6502

Signed32

Read/Write

Position